Four differences between QorIQ SDK V1.9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Four differences between QorIQ SDK V1.9

1,245 Views
xiaocheng
Contributor II

Question 1, what is the difference between the following four?

1. Cache: QorIQ SDK V1.9 PPCE500V2 CACHE
2. Image: QorIQ SDK V1.9 PPCE500V2 IMAGE
3. Source: QorIQ SDK V1.9 SOURCE
4. Virtual Host Enviroment: QorIQ DPAA SDK v1.9 PPCE500V2 with Virtual Host Enviroment

Question 2, I just want to use it to compile the uboot of the P2020 processor. It is as convenient as possible to build a development and compilation platform. Which one do you recommend?

0 Kudos
Reply
3 Replies

1,189 Views
yipingwang
NXP TechSupport
NXP TechSupport

1. Cache: QorIQ SDK V1.9 PPCE500V2 CACHE: includes the build Cache for e500v2 platforms to accelerate the building to avoid building anything from the scratch.
2. Image: QorIQ SDK V1.9 PPCE500V2 IMAGE:includes the pre-built image for e500v2 platform.
3. Source: QorIQ SDK V1.9 SOURCE: including recipes, source tar balls. 
4. Virtual Host Enviroment: QorIQ DPAA SDK v1.9 PPCE500V2 with Virtual Host Enviroment: is a virtual Linux environment including QorIQ SDK V1.9.

0 Kudos
Reply

1,189 Views
xiaocheng
Contributor II

hello Yiping Wang,

Thank you very much for your reply, maybe you said it very clearly, but unfortunately, I still can't understand the difference between them?

My worry is how to choose, in order to facilitate my own development environment.

0 Kudos
Reply

1,189 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please install both Cache and Source ISOs in the same path.

0 Kudos
Reply