Hi NXP supporting team,
I am facing one issue reagarding to the CAN_L and CAN_H volgtage when the TJA1043 devices is in sleep mode.
Attachment is the waveform i collected from oscilloscope.
It shows the CAN_L is from -1.5V to 0V, and CAN_H is from 0V to 1.5V, data decodes that is NACK error, represents that transceiver is in sleep mode.
So is it normal?
when receive the can frame from the bus, what's the voltage leverl for CAN_H and CAN_L?
In Sleep Mode the transceiver provides the following functions:
• The CAN transmitter is off.
• The normal CAN receiver is off.
• The local and bus wakeup function are active.
• INH is floating (lowest leakage current on INH pin).
• CANH and CANL are biased to GND.
• SPLIT is floating (lowest leakage current on SPLIT pin).