SRIO for P2040 processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SRIO for P2040 processor

661 次查看
arunthomas
Contributor I

Hi,

I'm referring "QorIQ P2040 Reference Manual, Rev. 4, 6/2016" for bring up SRIO for P2040 Processor.

On page 1255 under chapter - "Serial RapidIO Interface", there is a point that states - "RapidIO endpoint cannot be configured as four 1x or two 2x ports".

Does this mean we cannot use "SerDes Protocol Select" bits as 0xF, which configures for two 2x ports?

Do we have to use some other protocol which configures for 4x operation, if we are to use SRIO?

Regard,

Arun

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

432 次查看
Bulat
NXP Employee
NXP Employee

It is a typo, should be written "RapidIO endpoint cannot be configured as four 1x".

Regards,

Bulat