QorIQ eLBC Transfer Size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QorIQ eLBC Transfer Size

568件の閲覧回数
danialazo
Contributor I

P1020 QorIQ Integrated Processor Reference Manual, Rev. 6, 01/2013, Table 12-204 implies that with a “Word” Transfer Size and a “16-bit” Port Size, 32-bit data can be read from the 16-bit local bus, LAD[0-15].  It may also be implied that 32-bit data can be written to the 16-bit local bus, LAD[0-15].

The Port Size is set via the eLBC base registers.  However, other that the statement below, I have been unable to find a way to set the Transfer Size.  Please advise.

“The local bus always tries to transfer the maximum amount of data on all bus cycles”

Source: P1020 QorIQ Integrated Processor Reference Manual, Rev. 6, 01/2013, Section 12.5.3

ラベル(2)
0 件の賞賛
1 返信

468件の閲覧回数
ufedor
NXP Employee
NXP Employee

The transfer size is determined by a SOC master initiating a transaction to a eLBC target.

This means that eLBC does not alter transfer size of internal (platform) transaction.

For example, core, executing "stw", will generate 32-bit data write transaction.

0 件の賞賛