tag writer- password problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tag writer- password problems

925 Views
frank_fuchs
Contributor I

Hi, 

we tried to write a Tag with an "connect to WiFi" action. The tag should be protected.

Write to the tag fails every time when we add a password.

The same is for every action.

Any idea?

Frank

0 Kudos
Reply
4 Replies

694 Views
lisettelozano
NXP Employee
NXP Employee

Hello Frank, 

Could you please provide the NXP part number? 

Paulina

0 Kudos
Reply

694 Views
frank_fuchs
Contributor I

Hi,

there is no part number, as I am referring to your app.

The version # is 4.4

best regards

Frank

0 Kudos
Reply

694 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hello Frank Fuchs,

Hope you are doing great, I think that what Paulina asked is about what tag are you using, so we can replicate te problem or explain the correct procedure in case this works for us.

BR

Jonathan

0 Kudos
Reply

694 Views
frank_fuchs
Contributor I

Hello,

sorry for my late reply - I've been in vacation. 

The Tag I have used is a

"NFC Sticker, 22mm, NTAG 213, 180 Bytes, white"

from the NFC-tag-shop.de 

NFC Sticker Circus, 22 mm, NTAG 213, 180 Byte, weiß | NFC Sticker weiß & schwarz | NFC Aufkleber | N... 

hope you have an idea :-)

best

Frank

0 Kudos
Reply