sja1105 traffic Forwarding

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

sja1105 traffic Forwarding

238 次查看
haiyang
Contributor III

hi,

i use sja1105 to designe a switch ;

I want to implement a traffic forwarding function, all the traffic from port0 forwarding to port3,

What configuration should I do?

And i dont want  use vLAN ,is there a simple mirror function? 

best wish

标记 (1)
0 项奖励
回复
1 回复

218 次查看
kaden
NXP Employee
NXP Employee

Hi @haiyang ,

i do have a few questions to provide an appropriate answer.

Which variant are you using? SJA1105PQRS or the older SJA1105TEL? We recommend using the SJA1105PQRS for new designs.

Which tools are you currently using to generate a configuration for the device? 

BR

Kevin  

 

0 项奖励
回复