mc1322x reset modes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mc1322x reset modes

1,330件の閲覧回数
SteveJ
Contributor I
Hi,

I'm trying to figure out if it's possible to detect the reason for aprocessor reset on the mc1322x. Specifically I'd like to detect if areset was due to a POR, SW_RST or watchdog fail.Any ideas?

Thanks, Steve.
タグ(1)
0 件の賞賛
返信
1 返信

1,209件の閲覧回数
TomE
Specialist II

The ColdFire chips have a Reset Reason Register. The Power chips (MPC5604 anyway) has a "Functional Event Status Register". Kinetis have "System Reset Status" registers. If the ARM Core doesn't have this internally, this chip doesn't seem to have this available.

 

> POR, SW_RST or watchdog fail.

 

The code that performs the SW_RST could leave some "magic values" in SRAM somewhere, as long as there's some SRAM that survives a reset.

 

I've always tried to have a very high priority software watchdog running slightly ahead of the hardware watchdog. So if the software one triggers you know the hardware one is about to, and the software one can print where the code is stuck or record the stack frame somewhere. You could do the same (have the software one leave some different "magic" in SRAM).

 

Tom

 

0 件の賞賛
返信