maximun voltage in INT pin of RTC PCF8563

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

maximun voltage in INT pin of RTC PCF8563

Jump to solution
1,203 Views
diegoperez
Contributor II

Hi,

I am using RTC PCF8563 powered at 3.3V but would like to connect the INT pin to a 5V pull up. Is it suitable regardless the device is powered at lower voltage?

Thanks

0 Kudos
Reply
1 Solution
1,199 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Diego,

 

There will not be a problem as long the pull-up resistor is > ~500 Ohms.

Table 28.JPG

 

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
1 Reply
1,200 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Diego,

 

There will not be a problem as long the pull-up resistor is > ~500 Ohms.

Table 28.JPG

 

Best regards,

Tomas

0 Kudos
Reply