how to configure CAN gateway MC33665A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to configure CAN gateway MC33665A

457件の閲覧回数
Jeremy9602
Contributor I

See the registers map of the datasheet , to configura the GPIO function to satisfied my requirement, need to change the value of registers , but how to configure it? Is there any default project workspace or demo that could be refer to ? Thanks a lot 

0 件の賞賛
返信
1 返信

430件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The MC33665 driver and examples are part of the Automotive SW - BMS - Device Drivers SDK (for S32K3).

Capture.JPG

In case of PHY_665A, a set of four examples that configure the driver for status register reads with different configuration variants (SingleSPI with sideband signals, DualSPI with sideband signals, DualSPI without sideband signals, CANFD without sideband signal) is included.

And you might find useful the AN13640 "MC33665A SPI Application note" which is available as a Secure file (NDA required):

https://www.nxp.com/products/power-management/battery-management/battery-communication-ics/general-p...

Capture (1).JPG

BR, Tomas

0 件の賞賛
返信