Whether the HDMI interface of the IMX8MQ board supports the output timing of 8Kx1K@60HZ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Whether the HDMI interface of the IMX8MQ board supports the output timing of 8Kx1K@60HZ

1,546 Views
ximenbingmeng
Contributor III

We have reviewed the Data Manual and Reference Manual and see the following limitations 4K2K@60HZ,
But from the kernel source code, see, horizontal resolution and vertical resolution limits,
Therefore, please help to confirm whether the HDMI interface of the development board of IMX8MQ chip supports the output timing of 8Kx1K@60HZ, thank you very much!

Labels (1)
0 Kudos
Reply
2 Replies

356 Views
ximenbingmeng
Contributor III

I would like to know if the imx8mq(MIMX8MQ6DVAJZAB) chip also has the same limitations. When I use both HDMI and MIPI-DSI interfaces simultaneously, HDMI can only achieve 4K@30HZ ? Or rather, when I use both HDMI and MIPI-DSI interfaces simultaneously, HDMI can only achieve 4K@60HZ The MIPI-DSI interface can reach 1080p, thank you very much! Looking forward to your reply.

0 Kudos
Reply

1,522 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

For imx8qm hdmi support:

- HDMI -> 4K@60
For HDMI 4K@60 you have to combine DC0-0 and DC0-1, which means you lose MIPI-DSI0 and LVDS0,
conversely if you use either of those interfaces you are limited to HDMI 4K30.

It could not support 8k.

 

Regards

 

0 Kudos
Reply