Warning SGTL5000 : Not enforcing symmetric_rate due to race

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Warning SGTL5000 : Not enforcing symmetric_rate due to race

577 Views
alok
Contributor I

We have written one application in which we have created two pipeline i.e transmitter and receiver pipeline for audio . both the pipeline are not working simultaneously in the same process . At time only
one pipeline is working , when we are playing both the pipeline using thread then I am getting warning as
follows:
SGTL5000: Not enforcing symmetric_rates due to race

I also checked by running the command arecord | aplay I am getting same above error
SGTL5000: Not enforcing symmetric_rates due to race

Please help us to solve this problem , it is very critical for our customer.

0 Kudos
Reply
1 Reply

571 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alok 

 

unfortunately nxp does not support sgtl5000 in latest bsps, may be recommended to look and

test with boundary devices linux releases where that codec is used, as suggested on

https://community.nxp.com/t5/i-MX-Processors/Codec-SGTL5000-can-not-work/m-p/814506

 

Best regards
igor

0 Kudos
Reply