Urgent ,Why doesn't PTN3356 work ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Urgent ,Why doesn't PTN3356 work ?

1,679 Views
khhan
Contributor I

PTN3356 DisplayPort to VGA.

PTN3356 has ROM type and Flash type.

We used both  ROM type and Flash type, but didn't work.

We designed Schemetics that is copyed  NXP reference, so we think Schemetics is no problem.

Does it have to program? Does it  need a program using tool?

1) Crystal scope : 27MHz XTAL at power on,
oscilator about 1msec and  disappear 27M waveform.

2) Realtek's DP to VGA module:  It works well when we attach DP to VGA module to our DP port,

Mr Han , Solvitsystem.

0 Kudos
9 Replies

1,036 Views
akupchik
Contributor I

Hello,

I believe, we have a similar problem, Crystal  27MHz XTAL is not oscillating.  I will check if there is any clock activity following power up.

Please comment what was the root cause that you found.

 

Alex

 

0 Kudos

1,557 Views
khhan
Contributor I

Hi ,

Thank for your quick answer.

Our schematic is almost no proble.

At first , I would like to know need to program in PTN3356 like flash ROM .

Mr Han , in SOLVITSYSTEM

0 Kudos

1,557 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please check whether you schematic has a capacitor between SWOUT pin and PGND firstly!

0 Kudos

1,557 Views
khhan
Contributor I

Hi ,

OK , the 31 pin , SWOUT is connected 4.7uH input  ,and 4.7uH inductor output  is connected to 28 pin and CAP 4.7uF plus  0.1uF 3ea .

CAP out voltage , VDD 1.5V is OK .

Is it true that there is no need to program PTN3356 ROM or flash ROM using any down loading tools?

Thank for you response.

Mr Han .

0 Kudos

1,557 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

We have a DPCD tool attached, rar.file password is NXP

0 Kudos

1,370 Views
Gnimis
Contributor II

Hi,

Do you have the DPCD tool used under Linux?

0 Kudos

1,557 Views
khhan
Contributor I

Hi,

​I'm out of the office now.

I will check your response back to office.

Thank for your sincerely response.

Mr han.

0 Kudos

1,557 Views
khhan
Contributor I

Hi,

The Problem was cleared .

The problem is that Schemetic have missing point.

Thank you .

0 Kudos

1,557 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Please attached the schematic for us review!

Thanks!

BR

0 Kudos