UJA1169TK/X SBC wakeup by CAN and WAKE pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UJA1169TK/X SBC wakeup by CAN and WAKE pin

1,400 次查看
sivaEmbitel
Contributor II

Hello,

 

We have requirement, SBC is requested to have wake up via CAN and switch change of state on wake up pin.

The SW shall configure the following registers as below:

  • CWE bit from Transceiver event capture enable register (23h) shall be set to logic 1; (this will enable the CAN wake up mechanism)
  • WPRE bit from WAKE pin event enable register (4Ch) shall be set to logic 1; (this will enable rising edge detection on WAKE pin)
  • WPFE bit from WAKE pin event enable register (4Ch) shall be set to logic 0; (this will disable falling edge detection on WAKE pin).

 We observed that wake up by pin happens successfully, and we have a query on CAN standard wake-up

  • What is wake-up pattern, how we can send and how to test?

 

Please let us know how to send wake-up pattern and how to test wake by CAN

We are waiting for your response.

0 项奖励
3 回复数

941 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Siva,

In the datasheet, page 26, you can see the figure as below.

CAN wake-up.jpg

SBC needs to receive dominant->recessive->dominant sequence longer period than twake(busdom) and twake(busrec).within less than to(wake).

 

This should be more or less same for all CAN transceivers to wake-up by CAN wake-up pattern.

Best regards,

Tomas

0 项奖励

942 次查看
sivaEmbitel
Contributor II

Hello Tomas,

Thanks for your quick response,

we are facing a problem while putting SBC in to sleep mode.

We observed that SBC receives a Sleep mode command (MC = 001), it immediately switches to Reset mode. and 

  • Global event status register (address 60h) : SYSE (system event pending at address 0x61) bit is set,
  • We are trying to clear System event status register (address 61h): power-on (PO ) and watchdog failure (WDF) by writing 1 to corresponding bits but it is not clearing.

For reference find our observations below:

  • Read Command: 0xC100, Respose from SBC 0xC101
  • Read Command: 0xC300, Respose from SBC 0xC311

  • Read Command: 0xC500, Respose from SBC 0xC500

  • Read Command: 0xC700, Respose from SBC 0xC700
  • Read Command: 0xC900, Respose from SBC 0xC900

Let us to know any thing else need to configure other than these registers: 

  • We cleared the FNMC by programing non-volatile memory (NVM) registers (Software Development mode disabled).
  • SBC watchdog control register (0x00h) in WMC : Timeout, NWP: 128ms
  • Enabled the Transceiver event capture enable register (Write command: 0x4601)
  • Enabled WAKE pin event capture enable register (Write command: 0x9802)
  • Enabled CAN control register (Write command: 0x4001)
  • Enabled Mode control register (Write command: 0x0207) to enter in to Normal mode
  • Below is the schematic we have

pastedImage_2.png

Please help us to configure SBC in to sleep mode.

We are waiting for your response.

Regards,

Siva Sankar Chandika

0 项奖励

942 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Siva,

Enter to Sleep means V1 is OFF, then.

So, microcontroller may not have power any more.

If RSTN of microcontroller was connected to RSTN of UJA1169, microcontroller can set the pin low and UJA1169 is reset.

This can often happen in PCB design, but, this can only be solved by disconnecting RSTN of UJA1169 from RSTN of controller.

Best regards,

Tomas

0 项奖励