TJA1102 PHY_address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1102 PHY_address

286 Views
haiyang
Contributor III

hi,

i use the TJA1102 mow,

i reference the SPF-29837_B0-20.pdf  , i have some question.

NO1 question:

haiyang_0-1703843745222.png 

                                 Fig 1

whnen PHYAD[3:1]=100   why the P0_PHY ADDRESS is not 0x04?whether there have PHYAD[0]?

but i can't find it in datasheet.

NO2 question:

haiyang_1-1703843903688.png

                                   Fig 2

when PHYD[3:1]=100,why the P0 PHYADDRESS not same to the Fig1?

 

haiyang

best wish

Tags (1)
0 Kudos
Reply
1 Reply

258 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1) for PHY address explanation please refer to Table 20 of the DS

PetrS_0-1704201083200.png

2) here is typo in the schematic, PHYAD[3:1] should be 111, pull ups are used. Then PHY addresses are 0xE for P0 and 0xF for P1 

BR, Petr

0 Kudos
Reply