TJA1052i Questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1052i Questions

560 Views
prakashbhumired
NXP Employee
NXP Employee

Hi

Customer: Digilux Automation, India

For the isolated CAN transceiver (TJA1052i), is there below data (approximate) available?

  • Bus Loading
  • Length
  • Number of Nodes

I see the data is more less understandable from (https://www.nxp.com/docs/en/supporting-information/AH1014_v1_4_Application_Hints_TJA1042_43_48_51.pd... ) for the "no-isolated" ones.

Bur for TJA1052i, the app.note (https://www.nxp.com/docs/en/supporting-information/AH1301_Application_Hints_TJA1052i.pdf ) is not giving enough information.

Customer has below requirement:

They need a support upto 100 devices with a cable extendable up to 500 meters.

Any baudrade above 10kbps should be fine for their application.

Can someone comment on above questions &  if the TJA1052i can meet customer application?

BR

Prakash

0 Kudos
Reply
0 Replies