I would to know the difference between TJA1042T,118 and TJA1042T/1J;
/1J” is used to identify this device as the dual source version of the device. We internally manufacture this device at two FAB locations in order to give our end customer built in dual sourcing for many of our devices. This code is used for the EDI ordering only so there is no technical reason behind.
Had a look into the Q files and see there is a light difference in the content spec. Bonding wires differs as the weight of the die....and if weight of die differs ...any change in front end process?