TJA1021 tranceiver circuit diagram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1021 tranceiver circuit diagram

Jump to solution
1,922 Views
ykp3036
Contributor I

Is there any error in following Lin tranceiver TJA1021 circuit diagram?

ykp3036_0-1677649788239.png

When i use the S32K14 uart-lin, test will success.

But when i use the MPC5744P, test will fail and occurs bit error.

ykp3036_1-1677650115529.png

When i connect LINTX and LINRX, test will success.

So i suspect there is some error in my TJA1021 circuit diagram.

Could any one help me to check? 

0 Kudos
Reply
1 Solution
1,897 Views
guoweisun
NXP TechSupport
NXP TechSupport

我不清楚你是用的master 还是salve node,我给您的那个app note里面有电master 的电路也有slave的电路,有MCU TX/RX内部上拉,也有无内部上拉的推荐电路,您仔细看看会有所帮助。

 

View solution in original post

0 Kudos
Reply
8 Replies
1,904 Views
ykp3036
Contributor I

Sorry, i don't think this can help me solve problem

0 Kudos
Reply
1,921 Views
ykp3036
Contributor I

MPC5744 has the independent LIN module, S32K14 has the LIN in UART module

0 Kudos
Reply
1,908 Views
guoweisun
NXP TechSupport
NXP TechSupport

I attached the app note which has the typical application reference circuit of TJA1020.

Hope this could help you!
If any questions please let me know!

0 Kudos
Reply
1,904 Views
ykp3036
Contributor I

Sorry, i don't think this can help me solve problem

0 Kudos
Reply
1,898 Views
guoweisun
NXP TechSupport
NXP TechSupport

我不清楚你是用的master 还是salve node,我给您的那个app note里面有电master 的电路也有slave的电路,有MCU TX/RX内部上拉,也有无内部上拉的推荐电路,您仔细看看会有所帮助。

 

0 Kudos
Reply
1,902 Views
guoweisun
NXP TechSupport
NXP TechSupport

你有电话吗?我可以打一个电话给你

0 Kudos
Reply
1,887 Views
ykp3036
Contributor I

15262537495

0 Kudos
Reply
1,889 Views
ykp3036
Contributor I

大佬,加个微信,

 

yzqgymykp

0 Kudos
Reply