Simulating temperature effects on AWR models for the AFT09MS015N and AFIC901N

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simulating temperature effects on AWR models for the AFT09MS015N and AFIC901N

594 Views
petermcgill
Contributor I

Hi

I want to be able to simulate the effect of temperature on the Idq of my device using AWR. How can I achieve this using the device models for AFT09MS015N ad AFIC901N?

I see that the symbol for the AFIC901N has two pins called Vth1 and Vth2. How are these used?

Labels (1)
  • RF

0 Kudos
1 Reply

443 Views
andrei_skok
NXP Employee
NXP Employee

We do not have the thermal node connected for our models. Model is default at +25C.


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos