Dear All,
We have a custom board configured with 1.8V VDDIO, 1.8V VDDD and 3.3V VDDA. We can read and write to the chip via I2C. The I2S bus has all of the necessary signals, including MCLK, but we are unable to see any analog output on Line Out.
We are wondering if there is any aspect of the chip power supply configuration peculiar to 1.8V VDDIO and 3.3V VDDA operation that would impact this.
We are running with a 4.9 series Linux kernel on an NVIDIA TX2i module with the driver supplied with Jetpack 4.4.
Any hints appreciated.
David
解決済! 解決策の投稿を見る。
Hi,
I believe we have figured out what was going on. When we examined the power supply configuration code in the Linux driver, we saw the following (voltages here are given in mV):
if (vddio < 3100 && vdda < 3100) {
/* enable internal oscillator used for charge pump */
snd_soc_update_bits(codec, SGTL5000_CHIP_CLK_TOP_CTRL,
SGTL5000_INT_OSC_EN,
SGTL5000_INT_OSC_EN);
/* Enable VDDC charge pump */
ana_pwr |= SGTL5000_VDDC_CHRGPMP_POWERUP;
} else {
ana_pwr &= ~SGTL5000_VDDC_CHRGPMP_POWERUP;
/*
* if vddio == vdda the source of charge pump should be
* assigned manually to VDDIO
*/
if (regulator_is_equal(sgtl5000->supplies[VDDA].consumer,
sgtl5000->supplies[VDDIO].consumer)) {
lreg_ctrl |= SGTL5000_VDDC_ASSN_OVRD;
lreg_ctrl |= SGTL5000_VDDC_MAN_ASSN_VDDIO <<
SGTL5000_VDDC_MAN_ASSN_SHIFT;
}
}
As our intended VDDA supply was 3.3V, we did not require charge pump operation, so this branch was never invoked. The only other option supported, involving either VDDIO or VDDA exeeding 3.1V, then made a manual assignment of VDDC to the VDDIO supply. However, with our selection of VDDIO = 1.8V, this configuration would not allow the internal analogue switches in the SGTL5000 to operate. In other words, the stock Linux driver did not support VDDIO = 1.8V making it impossible for the device to produce audio output, despite appearing to operate correctly in every other sense.
On review of the SGTL5000 data sheet, it was apparent that an automatic voltage selection mode was actually supported, and the modified driver code snippet below was shown to reliably select VDDA as the source for VDDC in our configuration. This was confirmed by measuring 3.3V on pin 18 (CPFILT) of the chip.
if (vddio < 3100 && vdda < 3100) {
/* enable internal oscillator used for charge pump */
snd_soc_update_bits(codec, SGTL5000_CHIP_CLK_TOP_CTRL,
SGTL5000_INT_OSC_EN,
SGTL5000_INT_OSC_EN);
/* Enable VDDC charge pump */
ana_pwr |= SGTL5000_VDDC_CHRGPMP_POWERUP;
} else if (vddio >= 3100 && vdda >= 3100) {
/* Disable charge pump */
ana_pwr &= ~SGTL5000_VDDC_CHRGPMP_POWERUP;
/* VDDC use VDDIO rail */
lreg_ctrl |= SGTL5000_VDDC_ASSN_OVRD;
lreg_ctrl |= SGTL5000_VDDC_MAN_ASSN_VDDIO <<
SGTL5000_VDDC_MAN_ASSN_SHIFT;
} else {
dev_info(codec->dev, "SGTL5000 will choose highest voltage automatically!\n");
/* Disable charge pump */
ana_pwr &= ~SGTL5000_VDDC_CHRGPMP_POWERUP;
/* Switch to highest supply voltage */
lreg_ctrl &= ~SGTL5000_VDDC_ASSN_OVRD;
}
We now have audio output on LINEOUT as expected.
Hi,
I believe we have figured out what was going on. When we examined the power supply configuration code in the Linux driver, we saw the following (voltages here are given in mV):
if (vddio < 3100 && vdda < 3100) {
/* enable internal oscillator used for charge pump */
snd_soc_update_bits(codec, SGTL5000_CHIP_CLK_TOP_CTRL,
SGTL5000_INT_OSC_EN,
SGTL5000_INT_OSC_EN);
/* Enable VDDC charge pump */
ana_pwr |= SGTL5000_VDDC_CHRGPMP_POWERUP;
} else {
ana_pwr &= ~SGTL5000_VDDC_CHRGPMP_POWERUP;
/*
* if vddio == vdda the source of charge pump should be
* assigned manually to VDDIO
*/
if (regulator_is_equal(sgtl5000->supplies[VDDA].consumer,
sgtl5000->supplies[VDDIO].consumer)) {
lreg_ctrl |= SGTL5000_VDDC_ASSN_OVRD;
lreg_ctrl |= SGTL5000_VDDC_MAN_ASSN_VDDIO <<
SGTL5000_VDDC_MAN_ASSN_SHIFT;
}
}
As our intended VDDA supply was 3.3V, we did not require charge pump operation, so this branch was never invoked. The only other option supported, involving either VDDIO or VDDA exeeding 3.1V, then made a manual assignment of VDDC to the VDDIO supply. However, with our selection of VDDIO = 1.8V, this configuration would not allow the internal analogue switches in the SGTL5000 to operate. In other words, the stock Linux driver did not support VDDIO = 1.8V making it impossible for the device to produce audio output, despite appearing to operate correctly in every other sense.
On review of the SGTL5000 data sheet, it was apparent that an automatic voltage selection mode was actually supported, and the modified driver code snippet below was shown to reliably select VDDA as the source for VDDC in our configuration. This was confirmed by measuring 3.3V on pin 18 (CPFILT) of the chip.
if (vddio < 3100 && vdda < 3100) {
/* enable internal oscillator used for charge pump */
snd_soc_update_bits(codec, SGTL5000_CHIP_CLK_TOP_CTRL,
SGTL5000_INT_OSC_EN,
SGTL5000_INT_OSC_EN);
/* Enable VDDC charge pump */
ana_pwr |= SGTL5000_VDDC_CHRGPMP_POWERUP;
} else if (vddio >= 3100 && vdda >= 3100) {
/* Disable charge pump */
ana_pwr &= ~SGTL5000_VDDC_CHRGPMP_POWERUP;
/* VDDC use VDDIO rail */
lreg_ctrl |= SGTL5000_VDDC_ASSN_OVRD;
lreg_ctrl |= SGTL5000_VDDC_MAN_ASSN_VDDIO <<
SGTL5000_VDDC_MAN_ASSN_SHIFT;
} else {
dev_info(codec->dev, "SGTL5000 will choose highest voltage automatically!\n");
/* Disable charge pump */
ana_pwr &= ~SGTL5000_VDDC_CHRGPMP_POWERUP;
/* Switch to highest supply voltage */
lreg_ctrl &= ~SGTL5000_VDDC_ASSN_OVRD;
}
We now have audio output on LINEOUT as expected.
Dear David,
I have checked the supply values and they are within the recommended boundaries. Please find attached AN3663 and SGTL5000 Silicon Errata. In the Errata document is a description of an issue with an internal regulator not starting.
With Best Regards,
Jozef
Hi Jozef,
In relation to our earlier post about the lack of audio output from the SGTL5000 with Vddio = 1.8V, I should add that we have a Teensy breakout board running perfectly with Vddio = 3.3V using the same Linux driver code. Hence my question regarding special setup for 1.8V operation.
All clocks and data are being fed to the chip, with I2S data input to pin 25.
Can you confirm that customers are successfully using the SGTL5000 chip with Vddio = 1.8V?
Cheers,
David.
Dear Jozef,
Thanks for confirming the voltages. While running the SGTL5000 with
speaker-test -D hw:0,0 -c2 -r48000 -F S16_LE -t sine -f 1000
we see the following register values - Could you comment if you see anything that might prevent sound output from the Line Out (in view of the supply voltages)?
000: a011
002: 0061
004: 0008
006: 0130
00a: 0010
00e: 0200
010: 3c3c
014: 015f
020: 0000
022: 1818
024: 0022
026: 0020
028: 01f1
02a: 0000
02c: 0304
02e: 1f1f
030: 40f9
032: 5000
034: 0000
036: 0017
03a: 0000
03c: 0000
100: 0000
102: 0000
104: 0040
106: 051f
108: 0000
10a: 0040
10c: 0000
10e: 0000
110: 0000
116: 002f
118: 002f
11a: 002f
11c: 002f
11e: 002f
120: 8000
122: 0000
124: 0510
126: 1473
128: 0028
12a: 0050
12c: 0000
12e: 0000
130: 0000
132: 0000
134: 0000
136: 0000
138: 0000
13a: 0000
Best Regards,
David.
Hi David,
please see a reply from an application engineer I have contacted. Please see the description and AN3664 attached. Please provide the required information.
DESCRIPTION
Please refer to the AN3664. Which is the SGTL5000 chip package used in customer design? Could customer provide schematic to review please?
If SGTL5000 chip package which customer used in their design is 32QFN, please let customer check the CPFILT pin(pin connection) connection method in customer’s design as in the snapshot attached.
With Best Regards,
Jozef