SGTL5000 initiation and MCL question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000 initiation and MCL question

237 Views
uveuvenouve
Contributor I

Hi,

first , i want to ask if SGTL5000 can work without MCLK?
my purpose is to make a transparent headphone that just collect outside sound and play into headphone

if yes , is there any initiation code that about bypass mode without MCLK

thanks in advance!

0 Kudos
Reply
3 Replies

222 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi uveuvenouve,

SGTL5000 need an external oscillator connected to SYS_MCLK pin to work, and this should be between 8.0and 27MHz.

I have an SGTL5000 datasheet and SGTL5000 Initialization and Programming document, but these are confidential and can be provided under NDA only. (Non Disclosure Agreement). If you already have a valid NDA with NXP, please create a new case here. Please use your company email address and provide following information. 

Customer: ?

End Customer: ?

End Application: ?

Country: ?

Annual Volume: ?

If you haven't a valid NDA yet, and you would like to sign a new one, please create a new ticket here and our NXP representative for NDA matters will take you through the process.

JozefKozon_0-1721885403283.png

With Best Regards,

Jozef

 

0 Kudos
Reply

213 Views
uveuvenouve
Contributor I

Hi Jozef,

I want to make it clear so you mean it won't work without MCLK? right?

 

 

uveuve

0 Kudos
Reply

209 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi uveuve,

yes, correct.

With Best Regards,

Jozef

0 Kudos
Reply