SC16IS740: Will level change of /CS reset frame?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC16IS740: Will level change of /CS reset frame?

538 Views
dtmr
Contributor I

Will a high-low transisiton of the /CS signal of the SC16IS740/SC16IS760 reset the SPI frame, so that the chip will regard the next bit as the first bit of an SPI transmission?

I'm asking because I have no MCU pin left to control the reset line. If my MCU reboots, can toggling /CS get me out of an interrupted transmission (for software re-initialization)?

0 Kudos
2 Replies

479 Views
dtmr
Contributor I

Thanks.

0 Kudos

479 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

If CS signal is from low to high which mean SPI stop communication,SC16IS740 will wait for next effective command to do next operation which depend on the MCU code setting.

0 Kudos