S32R45 M7 bootloader downloads u-boot image from flash and activates A53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R45 M7 bootloader downloads u-boot image from flash and activates A53

21,537 Views
ssong
Contributor II

Following is the scenario we want:

** Flash Layout for boot **

---------------------------------------------------------------------------------------

Exported Blob                                                                                |

(IVT + QSPI reconf + DCD + HSE + Application bootloader(M7)) |

---------------------------------------------------------------------------------------

Application for M7                                                                          |

---------------------------------------------------------------------------------------

u-boot for A53                                                                                |

--------------------------------------------------------------------------------------

1. Application bootloader downloads Application for M7 and u-boot for A53

2. Application bootloader activates A53 and M7

3. u-boot in A53 configures hardware and downloads kernel for A53 from DRAM

4. u-boot jumps to kernel for A53

Is this possible scenario for S32R45? If so, can we make u-boot only image without IVT+QSPI reconf+DCD+HSE? What I found in mamual is the way of makeing u-boot image with them. Otherwise, Are there any other guided scenario for M7 bootloader to activate A53 in NXP?

Attached image is the S32DS bootsource configuration for better understanding

bootsource_m7.jpgbootsource_a53.jpg

23 Replies

3,623 Views
eddy_bts
Contributor III

Another question is that:

When we build ATF, we couldn't find a was to change fip image's load address.

It seems to be fixed as 0x34300980 as below. That's why we add FIP_MEMORY_OFFSET with 0x34300980.

eddy_bts_1-1654846101753.png

Can we change this address? Entry point might change accordingly.

 

0 Kudos
Reply

2,046 Views
ZhiguoZhong
Contributor I

Hello,

Have you successfully customized these two addresses?

About Load address and Entry point in ATF.

I have no idea about Load address...

 

 

0 Kudos
Reply

3,299 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

The load address is calculated depending on the size of dtb and a fip header (dummy_fip file). The image is built in the next way:

DUMYY_FIP_HEADER: Load address

DTB: BL2 address - DTB size

BL2 start and entry point at 0x3430_2000 

 

Saludos,

Alejandro

 

0 Kudos
Reply