Hello,
We are observing the S32N RTU0 core does not run and end in exception after a soft or hard reset on S32N EVB board with RTD version SW32NZ5x_RTD_R21-11_0.8.0_P01. The sw used in RTU0 is compiled with ‘-mthumb’ flag, we suspect that after RTU0 reset, core is running in A32 mode and not in T32. The Sw executes normally when .elf files are used since it has T32 mode enabled. Attached snapshots regarding the same. Let us know if this is already known.
Thanks.