S32DS3.5 无EmbSys Registers怎么查看 外设寄存器值

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.5 无EmbSys Registers怎么查看 外设寄存器值

Jump to solution
340 Views
jinsheng20
Contributor III

在中也没有发想现在有的发现没能查看外设寄存器值?请问我该怎么操作?

还有watch register 怎么用的有教程吗?

jinsheng20_0-1710843879523.png

 

0 Kudos
1 Solution
248 Views
jinsheng20
Contributor III

最后不确定什么原因,当时放弃查看了,后来过了两天外设寄存器界面可以看到寄存器值

View solution in original post

0 Kudos
4 Replies
249 Views
jinsheng20
Contributor III

最后不确定什么原因,当时放弃查看了,后来过了两天外设寄存器界面可以看到寄存器值

0 Kudos
324 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @jinsheng20 

S32DS version 3.5 does not have the EmbSys Registers view as older versions.

In this IDE version, you can use the Peripheral Registers, which is a view that provides the structured view of the peripheral registers on the target hardware. If Arm core registers are defined for the target device they are also present in this view. This view is included in the Debug perspective by default. If the view was closed, reopen it from the menu by selecting Window -> Show View -> Other -> Debug -> Peripheral Registers.

Also, there are other views available named Arm System Registers and Registers. The first view provides the structured view of the Arm System registers(if available) of the target hardware. The second view lists information about the registers in a selected stack frame. Values that have changed are highlighted in the Registers view when your program stops. You can use it to look into register details and change register values. 

 

B.R.

VaneB

0 Kudos
311 Views
jinsheng20
Contributor III

感谢你的回复

您描述的窗口也美誉任何信息,我怀疑是软件没有找到S32K344.svd文件。请问这个我该如何配置,我在NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\RTD\BaseNXP_TS_T40D34M30I0R0\header\目录中看到有S32K344.svd。请问软件默认查找路径是?

0 Kudos
304 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @jinsheng20 

The information provided by these views is available in Debug. The data are read from the registers of the RO (read-only) and RW (read-write) types at each debug action like a step, a resume, a stop, or a breakpoint.

0 Kudos