Problem when detect type B card using PN7150

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem when detect type B card using PN7150

916 Views
iwannugraha
Contributor III

Hi,

 

I tried to read type B card using PN7150 with Android-5.1.1 but can't detect at all and also using TagInfo application.

 

This is the log :

2022-12-04 09:26:54.913 754-1050/com.android.nfc D/NxpTml: PN54X - I2C Read successful.....
2022-12-04 09:26:54.914 754-1050/com.android.nfc D/NxpNciR: len = 4 > 600701A1
2022-12-04 09:26:54.914 754-1050/com.android.nfc D/NxpTml: PN54X - Posting read message.....
2022-12-04 09:26:54.914 754-1053/com.android.nfc D/NxpHal: read successful status = 0x0
2022-12-04 09:26:54.914 754-1053/com.android.nfc D/NfcAdaptation: NfcAdaptation::HalDeviceContextDataCallback: len=4
2022-12-04 09:26:54.914 754-1050/com.android.nfc D/NxpTml: PN54X - Read requested.....
2022-12-04 09:26:54.914 754-976/com.android.nfc I/BrcmNfcNfa: NFC received ntf gid:0
2022-12-04 09:26:54.914 754-1050/com.android.nfc D/NxpTml: PN54X - Invoking I2C Read.....
2022-12-04 09:26:54.914 754-976/com.android.nfc I/BrcmNfcNfa: nci_proc_core_ntf opcode:0x7
2022-12-04 09:26:54.914 754-976/com.android.nfc I/BrcmNfcNfa: nfa_dm_nfc_response_cback () NFC_GEN_ERROR_REVT(0x500d)
2022-12-04 09:26:54.914 754-976/com.android.nfc I/BrcmNfcNfa: nfa_dm_disc_data_cback ()
2022-12-04 09:26:54.914 754-976/com.android.nfc I/BrcmNfcNfa: nfa_dm_disc_sm_execute (): state: DISCOVERY (1), event: INTF_ERROR_NTF(10) disc_flags: 0x1
2022-12-04 09:26:54.914 754-976/com.android.nfc I/BrcmNfcNfa: nfa_dm_disc_sm_execute (): new state: DISCOVERY (1), disc_flags: 0x1
2022-12-04 09:27:16.305 754-1050/com.android.nfc D/NxpTml: PN54X - I2C Read successful.....
2022-12-04 09:27:16.305 754-1050/com.android.nfc D/NxpNciR: len = 4 > 600701A1
2022-12-04 09:27:16.305 754-1050/com.android.nfc D/NxpTml: PN54X - Posting read message.....
2022-12-04 09:27:16.305 754-1053/com.android.nfc D/NxpHal: read successful status = 0x0
2022-12-04 09:27:16.305 754-1053/com.android.nfc D/NfcAdaptation: NfcAdaptation::HalDeviceContextDataCallback: len=4
2022-12-04 09:27:16.305 754-1050/com.android.nfc D/NxpTml: PN54X - Read requested.....
2022-12-04 09:27:16.305 754-976/com.android.nfc I/BrcmNfcNfa: NFC received ntf gid:0
2022-12-04 09:27:16.306 754-1050/com.android.nfc D/NxpTml: PN54X - Invoking I2C Read.....
2022-12-04 09:27:16.306 754-976/com.android.nfc I/BrcmNfcNfa: nci_proc_core_ntf opcode:0x7
2022-12-04 09:27:16.306 754-976/com.android.nfc I/BrcmNfcNfa: nfa_dm_nfc_response_cback () NFC_GEN_ERROR_REVT(0x500d)
2022-12-04 09:27:16.306 754-976/com.android.nfc I/BrcmNfcNfa: nfa_dm_disc_data_cback ()
2022-12-04 09:27:16.306 754-976/com.android.nfc I/BrcmNfcNfa: nfa_dm_disc_sm_execute (): state: DISCOVERY (1), event: INTF_ERROR_NTF(10) disc_flags: 0x1
2022-12-04 09:27:16.306 754-976/com.android.nfc I/BrcmNfcNfa: nfa_dm_disc_sm_execute (): new state: DISCOVERY (1), disc_flags: 0x1

Labels (1)
  • RF

0 Kudos
Reply
1 Reply

807 Views
Hedashen
Contributor I

Hello. How did you solve this problem? I have the same problem now.

0 Kudos
Reply