PNEV5180B vs OM25180FDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PNEV5180B vs OM25180FDK

741 次查看
KsaK
Contributor I

Hello,

we want to buy Evaluation and Development Boards for PN5180.
The site offers 2 options for the NFC Frontend Dev Kit (PNEV5180B and OM25180FDK).
However, the descriptions of these products on the site:

OM25180FDK: It contains a PNEV5180B board with 65 mm x 65 mm antenna optimized for EMVCo applications, a 30 mm x 50 mm antenna with matching components optimized for NFC applications, three small antenna matching PCBs (approx. 30 mm x 50 mm sized) for implementation of a custom antenna matching circuit, an NFC sample card based on NTAG®216F (NFC Forum Type 2 Tag) and 10 PN5180 samples in HVQFN package.

PNEV5180B: link leads to OM25180FDK page

Please inform me about the actual configuration of the specified "NFC Frontend Dev Kit".

 

 
标签 (1)
0 项奖励
回复
1 回复

722 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi @KsaK 

Hope you are doing great, well in this case basically the OM is the full kit where you will have the EV board and other things like tags, smartcards, matching cirtcuit boards, a smaller antenna, etc. 

and the EV board is just the board in case you are not interested in the other components that you  can find in the OM. 

so basically both have the EV board but  one has more components and tags. 

 

 

Jonathan

0 项奖励
回复