PCA82C251- Resistance between CANH and CANL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA82C251- Resistance between CANH and CANL

726件の閲覧回数
AikangPhil
Contributor II

We bought two batch PCA82C251 chip:

Old batch:82C251Y /5504/D940

New batch:82C251Y /3502/D037

We faced the CAN communication problem with the new batch(82C251Y /3502/D037),and we measured the resistance between CANH and CANL ,The R=64KΩ,It's higher than the old batch(82C251Y /5504/D940),The R of old batch =37KΩ.

So we wonder the new batch (82C251Y /3502/D037) might be the fake chip ,could you please explain this for me, thank you very much.

タグ(1)
0 件の賞賛
返信
4 返答(返信)

719件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

HI

Please refer to datasheet parameter-Rdiff range is from 20K to 100K,you test result for two lot within this range,no problem for this ICs.

 

0 件の賞賛
返信

718件の閲覧回数
AikangPhil
Contributor II

Thank you very much for your answer. but we faced the communication problem, It looks the R may influence the communicate rate ? And we used the 37KΩ ICs without any problem for the past several years, How can we buy the selected 37KΩ ICs, does the factory have methods to control it? if possbile, you can call me to discuss it ,my phone: 13794495859

Thank you very much.

0 件の賞賛
返信

710件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

We can't control this parameter because they are within spec.

can you share with your schematic?

 

0 件の賞賛
返信

706件の閲覧回数
AikangPhil
Contributor II

Thank you very much, I will share this with our engineer.

タグ(1)
0 件の賞賛
返信