Only receiving 0xFF from NTAG 5 Link when reading registers over i2c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Only receiving 0xFF from NTAG 5 Link when reading registers over i2c

684 Views
Lukas5
Contributor II

Hello,

I already posted this issue, but i didnt receive an answer, maybe because the initial question in my Post was too long ago. So here is my Problem:

I am trying to set up my NTAG 5 Link. I want to set the ED-pin to change levels when an HF-field is detected. I am doing this like I read in the datasheet, I am writing the Value 0x01h to the register with the address 0x10A8h. When I check the ED-Pin with the 3.3 V connected to the Tag, the ED-Pin is at a level of 2,92 V.  The Problem is, when I try to put my phone on the tag, the level of the pin is not changing.

So I tried to read the register Value to check if it was written correctly. Now the problem: Whatever register I am trying to read on my device via i2c, I am always getting the Value “0xFF”. Why is that happening? Did I do anything wrong?

 

Would be really happy if someone could help me.

Kind Regards

Lukas

Tags (3)
0 Kudos
Reply
12 Replies

642 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please help me confirm that you are able to access those register via NFC?

 

Best Regards,

Ricardo

0 Kudos
Reply

626 Views
Lukas5
Contributor II

Hello Ricardo,

Hope you are doing well. I tried reading the registers via NFC using the "TagInfo" app and i was able to read the values of the registers. The value of register "A8" is "47 C7 67 17". The screenshot from my phone is attached.

This means there is probably a problem in the i2c-Communication, do you have any idea what it could be? Or could the problem be something else?

 

Best Regards,

Lukas

0 Kudos
Reply

610 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Lukas,

 

By any chance, were you able to read any other Register via I2C before?

 

Did you modify any other register?

 

Are you working with a development kit? Or is it a custom board?

 

Regards,

Ricardo

0 Kudos
Reply

527 Views
Lukas5
Contributor II

Hello Ricardo,

 

Hope you are doing well. I am sorry for posting again, but I really need a fast solution if possible, because I am a student and I need the NTAG for my Bachelor-Thesis. Without being able to read or write registers via i2c, I won't be able to finish in time, and I don't have much time left. It would be great if you would help me, because I don't know what the Problem is.

 

Kind Regards,

Lukas

0 Kudos
Reply

513 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello Lukas,

 

Could you please help me confirm that you are sending the correct frame?

Ricardo_Zamora_0-1720461474047.png

 

The communication should look like this:

Ricardo_Zamora_2-1720461502062.png

 

Best Regards,

Ricardo

0 Kudos
Reply

502 Views
Lukas5
Contributor II

Hello Ricardo,

thanks for your reply. My communication does not exactly look like yours. This is the screenshot of my communication:

Lukas5_0-1720501292311.png

I am using a HAL function to read from i2c, is this wrong?

Edit:

I just tried reading a different register, that is part of the user memory, i tried reading the register 0006h and i was able to get the bytes back. here is my log:

Lukas5_0-1720504121988.png

 

So the general reading process seems to be right, is there any reason that i cannot read the register 0x10A8h or the config registers in general?

 

Kind Regards,

Lukas

0 Kudos
Reply

469 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Lukas,

 

Please help me checking section 8.3.1.4 of the NTAG 5 link - DataSheet.

 

There you can check that the frame you would need to implement on your MCU, depending on the memory section you are trying to read/write. (user and configuration memory, or session registers).

 

Hope this helps!

 

Regards,

Ricardo

0 Kudos
Reply

345 Views
Lukas5
Contributor II

Hello Ricardo,

sorry for the late reply, I had trouble with posting a reply during the last days, because the button wasn't working.

I checked section 8.3.1.4 of the NTAG 5 link - DataSheet

The frame for writing according to the DataSheet hast to look like this:

Lukas5_1-1721035978606.png

 

I implemented the frame necessary for writing to the memory. I think i did it right, here is a screenshot of my i2c communication: 

Lukas5_0-1721035932167.png

However, i am only getting the Values "0x00 0x00 0x00 0x00" back instead of the actual Value of the register.

 

Kind regards

Lukas

 

0 Kudos
Reply

282 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Lukas,

 

Could you please try with the frame example I shared?

 

That is the frame you should use with this memory region.

 

Regards,

Ricardo

0 Kudos
Reply

269 Views
Lukas5
Contributor II

Hi Ricardo,

 

I'm not sure which frame you are talking about. You sent me this frame from your log:

Lukas5_1-1721714327627.png

 

and mine is looking like this:

Lukas5_0-1721714199687.png

I think it is looking the same until I want to receive data, because I am only getting 0x00 back, while you are receiving actual data.

 

It would be great if you could tell me, what exactly is wrong in my provided log, because I unfortunately have no idea.

 

Regards,

Lukas

 

0 Kudos
Reply

249 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Lukas,

 

Looks like there should be something with your host implementation.

 

The I2C communication works well on my side, for several NTAGS.

 

Regards,

Ricardo

0 Kudos
Reply

595 Views
Lukas5
Contributor II

Hello Ricardo,

I was not able to read any other register via i2c before; this was the result from the beginning when I tried to test the NTAG.

I did not modify any other register, as far as I know. I also tried writing a value to the register, but the value didn't change when I scanned the tag via NFC.

I am currently working with a development kit; it is not a custom board.

 

Thanks for your help so far, I hope there is a solution.

 

Regards,

Lukas

0 Kudos
Reply