NVT2008BQ LEVEL TRANSLATOR OPERATION

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NVT2008BQ LEVEL TRANSLATOR OPERATION

583 次查看
bijumohankc
Contributor II

We are using the level translator IC -NVT2008BQ in our design.But in our application , same voltage will be used at the both sides of the level translator in certain times (VADJ_1V8,it can be 1.2V or 1.8V). In datasheet its mentioned like "The applied voltages at Vref(A) and Vpu(D) should be such that Vref(B) is at least 1 V higher than Vref(A) for best translator operation." Could you please confirm whether this level translator can work with same voltages on both sides(Its not clear from the datasheet page.9) ? Or any other modification required for the following design which is attached with this?

0 项奖励
1 回复

507 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

This question is being solved internally (Case #00166169). 

0 项奖励