NTS0102 low level issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTS0102 low level issue

489 Views
tepper
Contributor I

Hello,

Relating to the datasheet of the NTS0102 the chip only accepts a low level voltage of 0.15 or less on its data inputs. This seems quite unusual for an CMOS chip and in addition it would contradict the information of the datasheet, that the ship is primary targeted for I2C applications because there the low level output voltage of chips is mostly in the range of 400mV. Is the given low level in the datasheet not correct or is this device not suitable for a I2C bus at all?

Best regards.

Tags (1)
0 Kudos
Reply
1 Reply

435 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

The device is primarily targeted at I2C or 1-wire which use open-drain drivers,so there is no error in spec.

But in I2C application,NTS0102's specification obviously more strict.

0 Kudos
Reply