MC56F8165 - Using FlashOverJTAG utility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC56F8165 - Using FlashOverJTAG utility

Jump to solution
1,650 Views
UsingMC56F8165
Contributor I
Hi
 
Is this the place for questions regarding the Usage of the FlashOverJTAG utility?
 
p.s. I'm using the MC56F8165

Message Edited by Alban on 2007-05-03 06:34 PM

0 Kudos
1 Solution
869 Views
william_jiang
NXP Apps Support
NXP Apps Support
i would suggest you use 56800E standalone flash programmer which can be downloaded from
 
The FlashOverJTAG will use internal program RAM, but 56F8165 has no such RAM.

View solution in original post

0 Kudos
1 Reply
870 Views
william_jiang
NXP Apps Support
NXP Apps Support
i would suggest you use 56800E standalone flash programmer which can be downloaded from
 
The FlashOverJTAG will use internal program RAM, but 56F8165 has no such RAM.
0 Kudos