Is there an example for PTN5110 with LPC55S69 + FreeRTOS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there an example for PTN5110 with LPC55S69 + FreeRTOS?

296 Views
csaba_finta_ext
Contributor I

The goal is to develop an application for LPC55S69+FreeRTOS with two PTN5110 chips where the MCU should control the current flow on VBUS (source/sink) between the two USB-C receptacles (ports A > B or B > A). Is there any driver, library or example with basic functions?

0 Kudos
Reply
1 Reply

281 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry as far as I know there is not sample code using the PTN5110

 

 

0 Kudos
Reply