Hello NXP team,
i wanted to include the docker engine for the imx93EVK board.
repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-nanbield -m imx-6.6.3-1.0.0.xml
above downloaded source in meta-virtualisation - I am not finding docker-ce folder when i added the below configs in local.conf
DISTRO_FEATURES:append = "systemd"
DISTRO_FEATURES:append = "aufs" DISTRO_FEATURES:append = "virtualization" IMAGE_ROOTFS_EXTRA_SPACE = "10000000"
CORE_IMAGE_EXTRA_INSTALL += "openssh"
EXTRA_IMAGE_FEATURES = "dev-pkgs debug-tweaks tools-debug ssh-server-openssh" IMAGE_INSTALL:append = "docker docker-ce connman connman-client net-tools iputils dhcpcd which gzip python python-pip wget cmake git gtk+ zlib patchelf nano grep tmux swig tar unzip parted e2fsprogs e2fsprogs-resize2fs"
TOOLCHAIN_HOST_TASK:append = "nativesdk-cmake nativesdk-make"
VIRTUAL-RUNTIME_init_manager = "systemd"
DISTRO_FEATURES_BACKFILL_CONSIDERED = "sysvinit" VIRTUAL-RUNTIME_initscripts = "systemd-compat-units"
let me know how to proceed. to build imx-image-core.
Thanks,
ranga
Hi @ranga_yn
The BSP has supported the docker layer . You can flash demo image and run 'docker' command after logging in the system.
Best Regards
Zhiming
Hello team,
could you please share me which demo image has to be flashed for docker to be working - link .
Thanks,
Ranga
Hi @ranga_yn
I just find that only imx8 series support docker in bb file, you can add below code in meta-imx/meta-imx-sdk/recipes-fsl/images/imx-image-core.bb
DOCKER:mx9-nxp-bsp = "docker"