IMX8mini PCB material

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8mini PCB material

875件の閲覧回数
idom
Contributor II

Hi 

I have a design with based on the IMX8mini with the LPDDR4, In your "i.MX 8M Mini Hardware Developer’s Guide" you  recommend PCB material TU768, but the PCB manufacturer only have S1000-2,TG170.

Do you see any problem if I change the PCB material?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

726件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

If the impedance matching it will be OK, but we still recommend you to use the HTG TU768,  because the HTG TU768 with low dielectric loss.

0 件の賞賛
返信

726件の閲覧回数
idom
Contributor II

Thanks for your answer,

Another question I have is about the stackup. There is a contradiction between the BRD file and MX8MMHDG.pdf.

In the BRD file the copper thickness is 1Oz but in hardware design guide it is 0.5oz. the problem is that there are 3mils traces on those layers. Hows did manage to manufacture it? Can I build the stackup with 0.5oz?

0 件の賞賛
返信