Hello,
To enable Keyfob avoidance on WCT-15WTXAUTO, I believe I need to set gHAL_bFobActive to "1".
When I modified this variable via "Variable Watch" window on FreeMaster (please see attached),
This variable seems to be correctly modified to "1", but charging doesn't start even if Rx was placed on Tx coil.
Could you advise me what registers I need to change to enable Keyfob avoidance in addition to gHAL_bFobActive ?
Note, gHAL_bDBGFobType and gHAL_wDBGFobDuration can't be modified from variable watch. (Read only)
Thanks,
Norihiro Michigami
AVNET
Solved! Go to Solution.
Hi, Norihiro,
If set gHAL_bFobActive to "1" when TX is not in power transfer state, TX will stick on off state. If set this variable in power transfer state, TX will change its operation frequency. For gHAL_bDBGFobType and gHAL_wDBGFobDuration, customer can set it read and write in FreeMASTER by themselves. Below is the description about keyfob variables, which can be searched in MPA9 application user guide.
BR
Xiangjun Rong
Hi, Norihiro,
If set gHAL_bFobActive to "1" when TX is not in power transfer state, TX will stick on off state. If set this variable in power transfer state, TX will change its operation frequency. For gHAL_bDBGFobType and gHAL_wDBGFobDuration, customer can set it read and write in FreeMASTER by themselves. Below is the description about keyfob variables, which can be searched in MPA9 application user guide.
BR
Xiangjun Rong
Hello Xiangjun,
Thank you for your answer.
I confirmed that the board worked as you explained.
Thanks,
Norihiro Michigami
AVNET
Hi, Norihiro Michigami ,
I have asked wireless charging team, because Chinese national festival is coming, it may take a long time to give you a feedback.
BR
XiangJun Rong