My ELF file size is 300 KB and the RAM size is 32 KB so i want to know what happens when i load a code in internal flash it will execute from the internal flash or it will send part by part to the RAM and execute from the RAM i am using MPC5554
never-displayed