Does the BGA2866 invert an input pulse?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the BGA2866 invert an input pulse?

606 Views
johneberly
Contributor I

I'm having trouble getting this question answered. I could purchase a Demoboard for the BGA2866, but the NXP website returns a demoboard for a BGU6010,2,etc. when I search and that is the wrong package.

Tags (1)
0 Kudos
Reply
1 Reply

543 Views
LPP
NXP Employee
NXP Employee

BGA2866 doesn't invert the input signal.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply