Does IMX6Q support e.MMC5.1?请问IMX6Q是否支持5.1版本的e.MMC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does IMX6Q support e.MMC5.1?请问IMX6Q是否支持5.1版本的e.MMC?

711件の閲覧回数
yang1769
Contributor I

The processor  is “MCIMX6Q6AVT10AD”,can it support the e.MMC5.1?

thank you!

Best regards!

0 件の賞賛
返信
3 返答(返信)

678件の閲覧回数
Serg_mx6
Contributor II

Hello, b45499, i have similar question related to using i.mx6 solo, is it necessary to do any hardware improvements when using eMMC 5.1 ICs? Regarding the correction of the mmc.c file, I read.

/drivers/mmc/core/mmc.c :

if (card->ext_csd.rev > 6) {              // The '6' has to be replaced with '7' For EMMC5.0

                                                        //  The '6' has to be replaced with '8'  For EMMC5.1

pr_err("%s: unrecognised EXT_CSD revision %d\n",

mmc_hostname(card->host), card->ext_csd.rev);

err = -EINVAL;

goto out;

         }

Questions:

1) In addition, in some cases it is necessary to change the settings of pins such as this:

#define USDHC_PAD_CTRL (PAD_CTL_PUS_47K_UP | PAD_CTL_SPEED_LOW | \
PAD_CTL_DSE_80ohm | PAD_CTL_SRE_FAST | PAD_CTL_HYS)

to:

#define USDHC_PAD_CTRL (PAD_CTL_PUS_47K_UP | PAD_CTL_SPEED_LOW | \
PAD_CTL_DSE_120ohm | PAD_CTL_SRE_SLOW | PAD_CTL_HYS)

Give a comment, is it necessary to do this?

2) Have you heard that some eMMC5.1 refuse to work without hardware improvements in the form of pulli up  EIM_DA3 (BOOT_CFG1 [3] bit) pin to 1 for working in normal mode?

Give a comment, is it necessary to do this?

Serg_mx6_0-1651489521921.png

Thanks

 

 

 

0 件の賞賛
返信

704件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The i.MX6Q support the emmc4.4, but the eMMC5.1 can work on it. You can use it.

0 件の賞賛
返信

650件の閲覧回数
Serg_mx6
Contributor II

Hello, b45499, Please answer if the described problems will appear?

0 件の賞賛
返信