Default SJA1110 config on BlueBox 3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Default SJA1110 config on BlueBox 3.0

73 Views
octave
Contributor I

Hi,

I have multiple BlueBox 3.0 with two different type of boards, SCH-47101 REV C and SCH-47101 REV D.

I am using the OVSP codedrop 0.8.0 image on the S32G.

 

With the rev C board, I can use the 1ge_P3 and 1ge_p4 port to communicate with the S32, no issues.

But with the rev D board, I can't even do a ping. The phy lights stay still when i try a ping from the CPU. But they do blink when I ping from a computer, so the PHY seems to be working.

I think it is a configuration issue between the CPU, SJA and PHY on the rev D board.

But I can't ping the SJA1110 on either board to flash it with TFTP.

 

What are the default configurations of the SJA1110 on the rev C and D Bluebox 3.0?

Can I flash them without using the JTAG ?

0 Kudos
1 Reply

27 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Please submit a ticket at NXP.com, or contact FAE/sales assigned to your company in order to further assistance.
Screenshot 2024-04-30 134950.png

Thanks for understanding.

BR, Petr

0 Kudos