Cockpit console issue with yocto build Image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cockpit console issue with yocto build Image

135 Views
bckpoojary
Contributor I

Hi,

I'm facing cockpit browser console issue in yocto builded image(6.1-mickledore) for i.mx8M nano ,I have added below mentioned cockpit image recipes into conf/local.conf file .but after the successful installation ,when accessing from browser using https://<ip_address>:9090 its showing below error,i have tried from updated browser also but facing same error,can anyone please help me on the issue?

 

This web browser is too old to run the Web Console (missing selector(:is():where()))

 

#IMAGE_INSTALL:append = " cockpit cockpit-pcp cockpit-tuned cockpit-shell cockpit-systemd cockpit-users cockpit-kdump cockpit-sosreport cockpit-selinux cockpit-playground cockpit-dashboard cockpit-bridge cockpit-ws cockpit-desktop

 

Thank you

 

0 Kudos
Reply
2 Replies

105 Views
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please share the steps that you did to compile your image?

Also, could you please share the processor you are using?

 

Thank you.

 

Best regards,

--... ...--

Salas.

0 Kudos
Reply

76 Views
bckpoojary
Contributor I

Hi @Alejandro_Salas ,

Thanks for your response.

I'm using i.mx8M Nano lpddr4 EVK with "imx-image-multimedia" image to compile.

added local and bblayer configuration file in below attachments.

 

Thank you

Regards

Bharath GC

 

 

0 Kudos
Reply