Can the MC33775A measure negative voltages, such as -2.78V, -3.33V?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the MC33775A measure negative voltages, such as -2.78V, -3.33V?

Jump to solution
266 Views
songhongyujl
Contributor II

I have two questions.
1. In the MC33775A datasheet, "Supports bus bars with ±5 V input voltage",can it be interpreted that it can measure negative voltage (such as -2.76V,-3.33V)?
2. What is the maximum number of MC33775A chips that can be connected in a daisy chain?
Thanks!

0 Kudos
Reply
1 Solution
233 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

It is possible that the voltage across the busbar is negative. The cell terminal inputs (CTx pins) of the MC33775A can handle negative voltages of up to −5 V. The cell balancing inputs (CBx pins) however can handle only −0.3 V.

MC33775A supports up to six daisy chains and 62 nodes per chain, please find more information in Application note AN13281

View solution in original post

2 Replies
234 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

It is possible that the voltage across the busbar is negative. The cell terminal inputs (CTx pins) of the MC33775A can handle negative voltages of up to −5 V. The cell balancing inputs (CBx pins) however can handle only −0.3 V.

MC33775A supports up to six daisy chains and 62 nodes per chain, please find more information in Application note AN13281

207 Views
songhongyujl
Contributor II

Thanks!!

0 Kudos
Reply