Automotive Ethernet to RJ45 Adapter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Automotive Ethernet to RJ45 Adapter

ソリューションへジャンプ
1,889件の閲覧回数
ethermike
Contributor II
I've just received my OM14510-SJA1105TJP: Automotive Ethernet Switch Application Board. The 4 PHYs are Automotive Ethernet connections but I would like to interface via RJ45 for development purposes. I checked with NXP support and there's no adapter available for sale. What's the best/cheapest/fastest way to convert Automotive Ethernet to standard RJ45 ethernet?
0 件の賞賛
1 解決策
1,813件の閲覧回数
ethermike
Contributor II

The most cheapest option I could find was the DP83TC811EVM from TI for $300. Kind of disappointed there aren't more reasonable options to facilitate automotive Ethernet development.

元の投稿で解決策を見る

0 件の賞賛
5 返答(返信)
1,814件の閲覧回数
ethermike
Contributor II

The most cheapest option I could find was the DP83TC811EVM from TI for $300. Kind of disappointed there aren't more reasonable options to facilitate automotive Ethernet development.

0 件の賞賛
1,862件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport
0 件の賞賛
1,853件の閲覧回数
ethermike
Contributor II

I'm looking for a more economical option. My hope was that NXP sold something like this to support development.

0 件の賞賛
1,880件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You mean converter between 100Base-TX to 100Base-T1?

 

0 件の賞賛
1,873件の閲覧回数
ethermike
Contributor II

Yes I believe so. The evaluation board I mentioned has two wire screw clamps for Automotive Ethernet on each of the four ports:

ethermike_0-1616684372117.png

I need to convert from the two line Automotive Ethernet to an RJ45 plug so I can use normal ethernet cables. I don't currently have any devices which use Automotive Ethernet.

0 件の賞賛