Analog voice scrambler PCD4440T

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Analog voice scrambler PCD4440T

744 次查看
chaitanyarobbi
Contributor I

In the PCD4440T data sheet the current consumption of the IC is mentioned as 10mA,but it takes 1mA only.

How to ensure that the IC is working fine or not?

I attached the PCD4440T test setup image.

In the datasheet "The time base for the PCD4440T is a 3.58 MHz input signal which can be derived from the oscillator output (OSCO) of Philips micro controller families PCD33xxA or PCF84CxxxA" is mentioned.Is it necessary to connect with Phillips micro controllers or we can interface with any other micro controller. If possible send the initialization routine or process.

Thanks in advance

Regards,

Chaitanya.

0 项奖励
0 回复数