About radar base on MR2001

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About radar base on MR2001

3,270 Views
thoomanwang
Contributor V

Radar system based on MR2001 chip is 1.5 ~ 2.5 meters can be detected and the high speed rolling diameter 10 mm long ellipsoid (length is more than 100 meters), according to the changes of the ellipsoid of short diameter return different signal strength? If you can, return measurement data can be less than 1 millisecond time?

2 Replies

605 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Thooman Wang,

Unfortunately the MR2001 radar device still under pre-production status and there are not documentation or information about it yet and therefore still not supported.

I apologize for the problems this may cause.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

605 Views
thoomanwang
Contributor V

Excuse me, what time will the formal launch of MR2001? Or open technical information.