Where retrieve correct BDM number for 'openbdm' in the TCL Interpreter?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where retrieve correct BDM number for 'openbdm' in the TCL Interpreter?

1,110 Views
rodrigon_hernan
Contributor III

Hello there,

I'm trying to follow a TCL script where the first line is "openbdm", but this just fails with "Illegal BDM number". The help content of the TCL Interpreter says the correct format is "openbdm [<deviceNum>]". I tried numbers that are show by firmware changer and the USB device ID numbers but without success.

Where to get this number or how to determine the correct number?

Attached is a screenshot of what firmware changer says about my USBDM.

Thanks !

0 Kudos
1 Reply

771 Views
pgo
Senior Contributor V

Hi Rodrigo,

Set the target type first and it will probe for suitable BDMs and list them with the BDM number.

e.g.

USBDMScript incorporating TCL - Copyright(c) 2011
Press ? for help


===============================================================
  usbdm_rc.tcl
================
  This file is 'sourced' whenever usbdmScript.exe is executed
  Add your own custom commands
===============================================================

% settarget arm
USBDM DLL Version = 4.12.1.150
BDM List:
 0 - USBDM-OPENSDA-3230891 : USBDM ARM-SWD for OpenSDA
Found 1 devices
:setTarget ARM
% openbdm 0
Opening USBDM-OPENSDA-3230891
BDM Version = HW=59, SW=4C

% connect
:connect
% reset
:reset 0x1C(DEFAULT, SPECIAL)
% regs
regs
  R0 => 00000000,   R1 => 00000000,   R2 => 00000000,   R3 => 00000000,
  R4 => 00000000,   R5 => 00000000,   R6 => FFFFFFFF,   R7 => 20002FF8,
  R8 => FFFEFFFF,   R9 => FFFFFFFF,  R10 => 1FFF3000,  R11 => 00000000,
 R12 => 00000000,   SP => 20003000,   LR => 00003647,   PC => 000004E8,
 PSR => 41000000,  MSP => 20003000,  PSP => FFFFFFFC,
FPSCR => 00000000, CONTROL/FAULTMASK/BASEPRI/PRIMASK => 00000000,
PC = 0x000004E8 : 0x02F0 0xF0FA
% rb 0 100
:rb =>
  0x00000000 : 00 30 00 20 E9 04 00 00 0D 2B 00 00 25 2B 00 00
  0x00000010 : 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
  0x00000020 : 00 00 00 00 00 00 00 00 00 00 00 00 0D 2B 00 00
  0x00000030 : 00 00 00 00 00 00 00 00 0D 2B 00 00 0D 2B 00 00
  0x00000040 : 0D 2B 00 00 0D 2B 00 00 0D 2B 00 00 0D 2B 00 00
  0x00000050 : 0D 2B 00 00 0D 2B 00 00 0D 2B 00 00 0D 2B 00 00
  0x00000060 : 0D 2B 00 00
0
%

bye

0 Kudos