USBDM problem using CodeWarrior 6.3 in windows vista x86

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM problem using CodeWarrior 6.3 in windows vista x86

1,188 Views
mandres
Contributor I

Hi, I am using an open source USBDM JM60 and I am trying to program a MC9S08JM 16, when I click on debug,  CodeWarrior displays a lot of warning messages and nothing happens with the microcontroller, this is not programmed at the end. I attached the screenshots of the warning messages, I do not know what's going on, I hope someone can help me.

The USBDM is recognized perfectly by the computer like a Libusb-win32 device.

Tags (2)
0 Kudos
Reply
1 Reply

370 Views
pgo
Senior Contributor V

Dear mandres,

 

What version of USBDM firmware and software?

Have you actually installed the DLL files?

Do you get the USBDM connection dialogue?

 

No suggestions are possible without the above information.

 

The dialogue provided don't really indicate much unfortunately - Just that codewarrior is having problems connecting to the target.

 

bye

 

0 Kudos
Reply