Dear All,
USBDM has been updated to V4.9.5
Please post any queries on this version in this thread,
Documentation available at: SourceForge
Applications available at: SourceForge
Source code is available at: GitHub
bye
Note
BDM History
V4.9.5a (July 2012) -
V4.9.5 (July 2012) -
Dear pgo, dear all,
I would like to know if JS16CWJ support programming of Flash and EEPROM for target :
HCS12 MC9S12DG256
S12X MC9S12XDP512
and with Coldfire V2,3,4 JS16 design, is it possible as well to program Flash and EEPROM.
MCF5235CVM150
I have read lot of threads and all the sourceforge project, a huge congratulation for all this piece of work.
Thanks,
Joe
Dear Joe,
the list of tested devices is somewhere on this page:
http://usbdm.sourceforge.net/USBDM_V4.9/USBDM_JS16/html/page_history.html
I believe the HCS12 devices you mention are amonst these.
MCF5235CVM150 should work with Codewarrior but the stand-alone programmer does not support it. It may be possible to add it but it depends on how similar it is to the ones already done.
bye
Hi,
I'm trying for the first time to get my BDM recognised by CodeWarrior.
The hardware is a Wytec BDM, supposed to be compatible with your software.
I downloaded your 4.9.5 msi and installed. No problems.
If I run HCS12_FlashProgrammer.exe to check if the hardware is recognised it tells me incompatible version, hardware is 4.9, software is 4.9.5. So I flash the hardware with 4.9.5, no problems.
Now I try to get Codewarrior to recognise the hardware, no joy.
The codewarrior version is 5.9.0, your site says files are for 5.1, is this a problem? Perhaps needed patches in codewarrior have not been done?
Regards,
Doug Jane.
Hi,
I've discovered my problem. You MUST install your MSI to the C drive. I previously installed to the E drive.
Bearing this in mind, the installer should not allow installing on other drives maybe?
Dear Doug,
I wasn't aware of any problems related to the installation directory but I suspect that's because it's not something I tried
The software does create a registery entry so that it can find the files wherever they are installed so there must be some problem I haven't anticipated.
Where the paths to the Codewarrior software correct in the installation?
bye
Yes, I had installed CodeWarrior to the C drive so the paths would have been as anticipated for that.
That'll teach me for trying to be smart. I have been installing a lot of programs to the E drive so that when Windows crashes and I need to do a clean install, I don't lose all my programs, but of course most programs using the registry don't work after the Windows reload. Oh for a better way! Linux?
Dear Pgo,
In your USBDM-CF hardware you've connector for Xilinx devices. Please tell me, how I can use this usbdm to program my Xilinx CPLD chip?
Thanks.
Regards,
Maciek
Sorry Maciek,
I added the connector because I was interested in the XIlink devices but I haven't done anything further.
bye
Awesome Job PGO, I'm doing some tests on secured SE8 chips, and I'm surprised, I thought that in order to enter BDM mode in a secured chip, a power toggle would be needed pulling the BKGD pin low, but I can se that my device is secured and the standalone programmer does not need to ask for a power off and power on to be able to reprogram the chip, how is it possible? !!
Dear carloscuev,
The device being secured doesn't have much affect on the connection success.
The only guaranteed way of connecting to a HCS08 or CFV1 device is through the the power-on-reset sequence you mentioned but in practice this is only necessary if one or more the of the following occurs:
bye
It worked! Thanks!
Rolling back to 4.9.4b fixes the issue
Dear Carlo,
Please see this link for a possible solution:
http://mcuoneclipse.wordpress.com/2012/05/21/fixing-the-morpho-core-exception/
It appears this error can be triggered by updating USBDM and other causes. I'm unsure why this occurs but the above procedure seems to fix it.
bye
Heelo PGO, I'm getting this problems when trying to debug an already existing proyect with USBDM target from previous version, I can't debug. I'm using 9.4.5b
An then, trying to make a new USBDM target:
Thank you very much for the S08 PA, PL and PT support !