Multiple OSBDM connections and CW10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multiple OSBDM connections and CW10

741件の閲覧回数
admin
Specialist II

I want to connect a couple boards via OSBDM. As far as I can judge, OSBDM is able to support multiple connected devices. But it looks like CW10 always connects to device #0, that is the first detected device, I guess.

 

What can I do with CW10 settings to make it debug another device (#1)? Is there any GDI connection attribute that may help here? I do not want to reverse-engineer the GDI dll really.

 

Thanks in advance

ラベル(2)
タグ(2)
0 件の賞賛
返信
0 返答(返信)