Hi SM,
I'm unsure if you are saying it didn't work or that the above list is incorrect?
The list given agrees with the description of the device i.e. 64 x 16K pages.
Please use the version USBDM_4_12_1_120_Win_b.msi as some version had a problem with paged addresses,
I did a partial test based on the above and it agrees with what was programmed into the device.
bye
I've read the mcu flash without any problems. I wanted to write the file i had read into a new mcu, but it wrote in the first time. After that it started to display the fault message 'target is secured'. Even though i did a mass erase, i can't write anything now. Why is this happening?
Hi SM,
The security of the device is determined by the image and the security options selected in the programmer. Did you select Unsecure before programming?
The Mass Erase Now button mass-erases the device. A mass-erased XEP is secured since the security area is blank. The Mass Erase Now button does not program the security area (to avoid wear on the chip).
You have to select the mass erase option for programming to a secured device:
I'm sorry the error dialogue is unclear.
Mass-erase is described here:
USBDM-Flash-Programmers: Flash Programmers Details
bye
Hi Sm,
I don't believe it is possible to read the paged EEPROM (from memory - I haven't done HCS12 stuff for years) as paging of EEPROM is not supported by the Memory dump utility.
To read the Flash you would need to define the following memory ranges (based upon the Project.prm file from a Codewarrior project):
All of the following would be 1 byte accesses:
Unpaged
4000 7FFF
C000 FFFF
Paged
C08000 C0BFFF
C18000 C1BFFF
C28000 C2BFFF
C38000 C3BFFF
C48000 C4BFFF
C58000 C5BFFF
C68000 C6BFFF
C78000 C7BFFF
C88000 C8BFFF
C98000 C9BFFF
CA8000 CABFFF
CB8000 CBBFFF
CC8000 CCBFFF
CD8000 CDBFFF
CE8000 CEBFFF
CF8000 CFBFFF
D08000 D0BFFF
D18000 D1BFFF
D28000 D2BFFF
D38000 D3BFFF
D48000 D4BFFF
D58000 D5BFFF
D68000 D6BFFF
D78000 D7BFFF
D88000 D8BFFF
D98000 D9BFFF
DA8000 DABFFF
DB8000 DBBFFF
DC8000 DCBFFF
DD8000 DDBFFF
DE8000 DEBFFF
DF8000 DFBFFF
E08000 E0BFFF
E18000 E1BFFF
E28000 E2BFFF
E38000 E3BFFF
E48000 E4BFFF
E58000 E5BFFF
E68000 E6BFFF
E78000 E7BFFF
E88000 E8BFFF
E98000 E9BFFF
EA8000 EABFFF
EB8000 EBBFFF
EC8000 ECBFFF
ED8000 EDBFFF
EE8000 EEBFFF
EF8000 EFBFFF
F08000 F0BFFF
F18000 F1BFFF
F28000 F2BFFF
F38000 F3BFFF
F48000 F4BFFF
F58000 F5BFFF
F68000 F6BFFF
F78000 F7BFFF
F88000 F8BFFF
F98000 F9BFFF
FA8000 FABFFF
FB8000 FBBFFF
FC8000 FCBFFF
FE8000 FEBFFF
This is untested.
bye