JS16 ICP Bootloader fails on newer versions since 4_12_1_140

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JS16 ICP Bootloader fails on newer versions since 4_12_1_140

960 Views
mculater
Contributor III

Builds 150 and 160 both fail when attempting to program a blank JS16 chip, producing the following error message:

---------------------------
Programming Error
---------------------------
Programming Failed   
Reason: USB connection with BDM has failed.

When I roll back to build 140, it works properly.  Tried builds 150 and 160 also with the latest USBDM driver installed, resulting in the same error message being displayed.

0 Kudos
2 Replies

681 Views
pgo
Senior Contributor V

Hi Carl,

I believe I have located the error.  This will be fixed in V4.12.1.170.

Please check after it is released.

bye

0 Kudos

681 Views
mculater
Contributor III

Thanks Peter!

0 Kudos